Other Parts Discussed in Thread: ADS1258, REF2025, BUF634
Hello,
1. We want to measure 16 sensors single ended with the ADS1258. The sensors are configured as a quarter bridge with the circuit taken from the TI example below. R10 being the sensor element in the bridge. With the given VREFP of +2.5V and supply voltage of +5V, the bridge circuit delivers a voltage range from above +0V to below +5V. VREFN is GND. We hope this is reasonable?
The Reference we use is REF2025, with a Buffer to supply the 16 bridges BUF634.

Single-Supply Strain Gauge Bridge Amplifier Circuit (Rev. A) (ti.com)
2. We are not sure what to do with AINCOM? Does this has to be +2.5V? And thus VREFP +5V?

Thanks a lot