This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using DAC161S997EVM evaluation board.
I am trying to connect this board with my PC but the DAC161S997 GUI software is showing this pop-up.
Please give the solution ASAP.
Thank You.
Hi,
A few questions:
1. Can you try running the GUI as an administrator?
2. Go to Device Manager and see the EVM is detected there or not?
3. Which version of OS are you running? This EVM is tested only up to Win 7.
4. How do you have the power connected to the EVM?
Thanks,
Lucas
Hi,
Answers of your questions are:
1. Yes, I tried to run GUI as an administrator.
2. Yes, EVM is detecting in device manager with COM25.
3. I am using Windows 10 Pro OS.
4. I applied 24V power supply at J1 connector with 100 Ohm series resistor.
Thank you.
Hi,
I would make sure you have the Labview Run time engine version 2014. Can you download it from the below link and try it?
32 bit:
64 bit:
Thanks,
Lucas
Hi,
I installed Labview Run-Time Engine version 2014.
Could you please tell me the further process.
Thanks
Hi,
DAC161S997 GUI is loading correctly but I am trying to connect DAC161S997 EVM then it is showing a pop-up.
Thanks
Hi,
Are you powering the DAC by shorting the the 2 pin header labeled DAC_CUR1 and VDD?
Thanks,
Lucas
Hi,
Can you try downloading the NI-VISA driver from: http://www.ni.com/download/ni-visa-17.0/6646/en/
Download the 17.0 version and try to use the GUI again, if this doesn't work, download the latest version.
Please let me know if this works for you.
Thanks,
Lucas