Hi TI-Support Team
We are looking for a solution on how to filter 50/60Hz noise from a SIL2 anlog 4-20mA loop signal. But to be honest im not sure if this is a bit to much for just filtering 50/60Hz from an anlog signal. Our required AC performance is only 20Hz. So my questions are: What would be the best filter ind the ADS127L21 for that application (SINC1+ SINC3, FIR1 etc.)? Do I need a external oscillator or can I use the integrated clock? If needed how do I calculate the FIR/IIR coefficients? If i activate the SPI CRC in the CONFIG3 register do I need to send a CRC with that command already or only with all subsequent massages?
I do have a EVAL board already.
Thanks in advance.
Regards Theo