About DACx311Series Device, do they have P/U resistors or P/D resistors each inside?
Three terminals are follows. If exists, how many kΩ are there?
And also do they have diode of ESD protection?
a)SYNC/
b)SCLK
c)Din
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
About DACx311Series Device, do they have P/U resistors or P/D resistors each inside?
Three terminals are follows. If exists, how many kΩ are there?
And also do they have diode of ESD protection?
a)SYNC/
b)SCLK
c)Din
Thank you.
Hello,
There are no internal pullup resistors on the input pins. The three digital input pins you mentioned have ESD cells that start conducting when the voltage on the pin is 0.3V greater than VDD. This is the reason for the absolute maximum ratings being VDD + 0.3V.
Best,
Katlynne Jones