This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: data read from ads1298

Part Number: ADS1298

Hi,

I am using ADS1298 IC for ECG data. I am using STM32 to communicate with ADS1298. The SPI communication is successfully happening between these two. My doubt is that , from which register I need to read the ECG data. When I checked in the datasheet every registers are meant for configuring/setting channels expect LOFF_STATP and LOFF_STATN (which is read only). As per my understanding CHnSET registers are for setting up each channels. So can anyone tell me which is the register (register name or datasheet page no.) where the ECG data as such can read? 

Regards, 

Neelima S