Part Number: ADS7038-Q1
Hello ,
I have configured the device to work in "On the Fly Mode". Also enabled CRC and status appended. I am getting CRC error in the 4 Bit "Status" that I am getting in the received frame. I tried the following 2 scenarios
1. Appended the CRC of the 3 Bytes and appended the CRC in the 4th Bit in the TX Frame. The 4-bits Status in the LlswADS7038RxBuf always gives "0x0A" which implies CRC error

2. Appended the CRC of 12 bits = '1' + '4-Bit' channel ID +0 and appended in the end. Still getting CRC error

NOTE: Even with the CRC error I am continuously getting the ADC values
Need support on how the SW calculated CRC needs to be calculated and appended in the TX frame in On the fly mode.