This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8760: Question about a device like DAC8760 which has internal DCDC converter to reduce dissipation power of IOUT circuit.

Part Number: DAC8760
Other Parts Discussed in Thread: DAC8771

Hello guys,

One of my customers uses DAC8760 for 4mA-20mA interface of their current mass-productions.

At this moment, they have the following question.
Could you please give me your reply?

Q.
They are in trouble of heating issue of the device when IOUT is 20mA.
For countmeasure, they are considering to replace DAC8760 with other company IC which has a internal DC/DC converter to adjust the power supply voltage of IOUT constant current source to appropriate one for reducing power dissipation.

Does TI have such device? Or do you have any plan to release such device?

Your reply would be much appreciated.

Best regards,
Kazuya.