In 7.3.27 of SLASE17B an equation is given to calculate IOUTFS. It is dependent on VEXTIO which is the same as VREF if the internal reference is used. Is there any way to determine a tolerance for IOUTFS given that only a typical value (0.9V) is specified for VREF?