Hi all,
I'm working with DAC3283 device on a new project. The device is assembled in a PCB with an FPGA and DSP devices.
I'm trying to configure the DAC with SPI interface but there are some issue.
First of all I have setted the DAC SPI in 4 wire mode setting the bit2 (sif4_ena) of CONFIG23 register after that I can see, on the logic analyzer connected on the SPI bus, the MISO data outgoing both SDIO and SDO/Alarms PINs.
This test lets me to understand that I have write correctly the CONFIG23 register. If I try to read back the same register I read a wrong values?
Any idea about this issue?
Thanks in advance.