Section 8.5.2.1 in the TLA2024 data sheet only shows I2C reads using stop followed by start (after the register pointer and before the read command). However in the I2C timing requirements, section 7.6, there are values for repeated start conditions. Is it legal to read a register in the TLA2024 using a repeated start instead of two separate commands?