Part Number: DAC3283
Hi,
I saw a forum post earlier mentioning about using this DAC to support two real data inputs. It mentioned that I should not use the complex mixer or QMC functions.
I am wondering which registers I need to setup for only "real" data operation? I want to confirm that If I leave bit 1 and bit 0 of CONFIG0 register (mixer_func) set to "00" then it should bypass the complex mixer. I also want to confirm that if I leave any QMC related registers set to default "0" then the data signal would also bypass those functions as well?
Lastly, will this process work if I input two different real data signals into the 16 bit "I and Q" data (of course in the 8 bit format with rising and falling clocks) and then get those two different real data signals to come out of IOUTA1 & IOUTA2 (I am assuming this is what "i" data is) and IOUTB1 & IOUTB2 (I am assuming this what "q" data would be)?
Thanks,
Jason