Hi All. I am in trouble with this device. more than a week I fight and result steel same.
This is custom board , have a little noise on supplies.
VCAP voltages :
VCAP1 : 1.2V
VCAP2 : 1.37V
VCAP3 : 4.68V
DVDD: 2.80V
AVDD: 2.77V
(https://github.com/RobertCsordas/MobilECG-II) this design.
anyone can advice what have to check?
internal test signal
RLD, LL(CH3), LA(CH2), RA(CH2N-3N), and CH4 on chest.