Hi,
I am using ADS131M08QPBSRQ1 in my design. Its internal reference is only 1.2V which is very low and impose a lot of constraints to my design. I have these questions:
1- What is the maximum reference voltage that can be applied to REFIN pin of this ADC? Can I supply this pin with a 3.3V reference voltage?
2- What is the recommendation on supplying this chip? Should I connect DVDD digital supply to a typical 3.3V and the analog supply AVDD and REFIN pin should be connected to my high precision 3.3V reference voltage?
3- If I connect my analog supply AVDD and REFIN pin to a 3.3V reference chip, what is the required current to supply these pins from the reference chip?
Thanks