Part Number: DDC232
Hello!
I have been testing the DDC232 board with a short molex cable (~10cm), a long molex cable (~50cm) and a usb C. Everything else remains the same, but when switching the cables to acquire data I have came across some issues with the read-back pattern. With the short molex cable everything works as expected, as I obtain the configuration register, the test pattern, some zeros and then these values are repeated. However, when I use the long molex the configuration register is wrong, as well as the test pattern and the repetition is not true because two of the characters changed (from 0 to 8 in both cases). Finally, on the usb C the test pattern is also different to the expected, the repetition is not true and the configuration refgister is only correct the first time. I copy below the read-back information I receive in each scenario in case anyone can help me find out what is happening.
Short Molex:
1801000000000000000000000000000000000000000000000000000000000030F066012480F69055
1801000000000000000000000000000000000000000000000000000000000030F066012480F69055
Long Molex:
0C0080000000000000000000000000000000000000000000000000000000001878330092407B482A
8C0080000000000000000000000000000000000000000000000000000000001878330092407B482A
Usb-C:
1801000000000000000000000000000000000000000000000000000000000030706601A400F61055
9801000000000000000000000000000000000000000000000000000000000030F06601A480F69055
Thanks in advance,
Sonia