This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I can find the reference design for ADC12D1X00, but is there same document specifically for ADC12D1600RB? If so, where to download?
Thanks,
Hi Alex,
The design files for ADC12D1600RB can be found on the product page for ADC12D1600RB. Here is a link to the design and development section of the page which contains the files. This design supports the ADC12D1000, ADC12D1600 and ADC12D1800 devices which are all just different speeds of the same ADC. https://www.ti.com/lit/zip/snac039
Thanks, Chase
Hi Chase,
Thank you for the quick reply. I did find the reference design in snac039.zip, but it is for "ADC12D1X00" and looks a bit different with ADC12D1600RB. So I wanted to confirm if there is a one specifically for ADC12D1600RB.
Best,
Hi Alex,
There is no difference in the reference design aside from the part swapping of the ADC. It can be used as reference for any of the ADC12D1x00 devices. If there is any specific questions you have towards tailoring a matching network, etc, then we are more than happy to help with that, but this design should act as a good start point.
Thanks, Chase
Hi Chase,
A follow-up question about the design layout in snac039. Comparing with the ADC12D1600RB, there are some differences, e.g. U11 relay in diagram can not be found on board, EXT CLK is supposed to be J11 in the diagram, but there is no R180 in it. It seems A side of R180 is not implemented for EXT CLK, so the external clock can not be used. Is there any way to use the external clock?
Best,
Hi Alex,
I think I have found what the issue may be - I believe the files are outdated. Please try with the below file.
3771.ADC12D1X00RF_RB-SCH_B.pdf
Thanks, Chase