The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC11001B: DAC recommendation for SMU

Guru 10450 points
Part Number: DAC11001B

Hello,

My customer is looking for a precision DAC that satisfies the following conditons for SMU(Source measurement unit) application.

   - Resolution : 24Bit

   - Sample rate : 1Msps or higher

   - I/F : SPI or I2C

   - Additional option : R2R Architecture, Output +/- both supported

Could you please recommend the best product that best meets the conditions?

Thank you.

JH

  • Hi ,

    Currently DAC11001B is the best DAC in the industry with 20bit, 1 MSPS resolution which is suitable for SMU applications.

    Having said that, we do have new device which is a parametric measurement unit suitable for SMU applications ( highly integrated device with force and measure functions )

    Can you connect with me through email?

    a.k@ti.com

    Regards,

    AK