Other Parts Discussed in Thread: INA849, TPS65130, INA851, TPS7A39
Hello,
I am starting a new design for an acquisition system with up to 32 channels isolated to each other. Each channel block will have an isolated DCDC and an ADS127L11 ADC. I am now at the stage that I would like to define the front-end for the ADS127L11 and I am facing some design changes and would like to ask about your recommendation for possible setups. Below you can find the requirements:
- As each channel is isolated from each other I do not have any excessive CMMR requirements
- Input impedance of 1GOhm
- Measurement range of +/-10V
- If possible the output of the isolated DCDC should be 5V
Looking at the requirements the most obvious choice could be an INA instrumentation amplifier. The issue is that I would need bipolar supplies. I am wondering, as I have seen in other commercial products with exactly the same requirements with the exception of the usage of a 16bit ADC and without instrumentation amplifiers, if there is a way either to avoid the bipolar supplies or to generate them out of the 5V main supply in a very simple way. I have a very small space in layout for each one of the channels and therefore area is of the essence. Furthermore the instrumentation amplifiers tend to be quite cost intensive.
Thanks in advance for your support and Best Regards,
Javier