Hi,
I am working on THS1206 ADC interfaced to FPGA (XC7A75TFGG676-2L). The 2 control registers programmed as: CNTR0 = 0x0C8 and CNTR1 = 0x410. When I am reading the data from the ADC for both the channels data out is same. The 2 inputs are connected as: AINP-AINM with differential sine wave with 3 kHz of 1.2 Vpp and BINP-BINM are shorted i.e., 0V. I tried keeping both these differential inputs open then also both outputs are appearing same.
I am adding screenshot for your reference which the case when channel A is differential input and channel B is shorted. The CONV_CLK is 6 MHz. DATA_AV is togging but it's not periodic. Would you let me know why am I getting same output value for both differential channels? Why DATA_AV doesn't toggle periodically?
Thanks