Hi everyone,
I would like to calibrate the gain of the ADS131. The datasheets mention some internal test signals in section 8.3.9. Apart from the fact that these test signals are +/- 2 / 15 * Vref, there is not much more information.
Therefore, can anyone let me know if these signals can be used for internal gain calibration?
How accurate/reliable are these signals?
Do these signals vary from device to device or even from channel to channel?
Thank you in advance and best regards
Daniel