Part Number: ADC12DJ5200RFEVM
Other Parts Discussed in Thread: ADC12DJ5200RF, TI-JESD204-IP
Hi,
Now, I am puzzled by the gap between the datasheet and the reference design.
How is the JMODE1 data format handled in the transport layer?
The following is an excerpt of comments from the transport layer source code included with the reference design (SLWC120).
SourceFile:transport_ADC12DJxx00.v
// Bit pattern for JMODE1. Please refer ADC12DJxx00 datasheet for more details // Bit packing format is same for both JMODE1 and JMODE3. Please view this verilog file in notepad++ to have proper alignment of the table shown below // On 3rd link clock, 40 samples from first half of first frame is sent out- [S0, S1,.., S39] with S0 as MSB in rx_dataout signal // On the 4th link clock, 40 samples from second half of first frame is sent out- [S40, S41,.., S79] with S40 as MSB in rx_dataout signal // On the 5th link clock, 40 samples from the first half of second frame is sent out- [S0, S1, S2, …, S39] with S0 as MSB in rx_dataout signal and the sequence repeats // Out samples are delayed by 3 link clocks, due to internal registering /* s0 31:20 s16 19:8 s32 7:0 31:28 s48 27:16 s64 15:4 3:0 s2 63:52 s18 51:40 s34 39:32 63:60 s50 59:48 s66 47:36 35:32 s4 95:84 s20 83:72 s36 71:64 95:92 s52 91:80 s68 79:68 67:64 s6 127:116 s22 115:104 s38 103:96 127:124 s54 123:112 s70 111:100 99:96 s8 159:148 s24 147:136 s40 135:128 159:156 s56 155:144 s72 143:132 131:128 s10 191:180 s26 179:168 s42 167:160 191:188 s58 187:176 s74 175:164 163:160 s12 223:212 s28 211:200 s44 199:192 223:220 s60 219:208 s76 207:196 195:192 s14 255:244 s30 243:232 s46 231:224 255:252 s62 251:240 s78 239:228 227:224 s1 287:276 s17 275:264 s33 263:256 287:284 s49 283:272 s65 271:260 259:256 s3 319:308 s19 307:296 s35 295:288 319:316 s51 315:304 s67 303:290 291:288 s5 351:340 s21 339:328 s37 327:320 351:348 s53 347:336 s69 335:324 323:320 s7 383:372 s23 371:360 s39 359:352 383:380 s55 379:368 s71 367:356 355:352 s9 415:404 s25 403:392 s41 391:384 415:412 s57 411:400 s73 399:388 387:384 s11 447:436 s27 435:424 s43 423:416 447:444 s59 443:432 s75 431:420 419:416 s13 479:468 s29 467:456 s45 455:448 479:476 s61 475:464 s77 463:452 451:448 s15 511:500 s31 499:488 s47 487:480 511:508 s63 507:496 s79 495:482 483:480 */
According to comments, LSB=> S32、MSB=>S15

but, the ADC12DJ5200RF data sheet says that data is sent MSB first.

So I would think that MSB and LSB would be as follows.
LSB=> S0、MSB=>S47

For example, I think the test pattern for the short transport layer will look like this.

What is the right thing to do?
I'm sorry I didn't make it clear enough.
Regards,
Takeo