Hi, team
Please teach me how to adjust the TRIG_IN voltage.
I would like to make the external trigger input voltage even smaller than 1.8V.
The manual(slwu092) says it is adjustable, but I could not find a specific way to do this.
>3.3.3.1 SMA Connectors
>J13 TRIG_IN Adjustable level CMOS trigger input. Default level is 1.8 V
Can I change TRIG_IN voltage in the GUI?
Do I need to modify the hardware (EVM)?
Regards,
Takeo