Hello ,
What would be the maximum output voltage range of DAC if VCC is 3.3V , as Vref is 2.5V and if we select a Gain of 2 , can we expect Vout to range from 0 to 5V.
Please provide the feedback!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello ,
What would be the maximum output voltage range of DAC if VCC is 3.3V , as Vref is 2.5V and if we select a Gain of 2 , can we expect Vout to range from 0 to 5V.
Please provide the feedback!
Hi Asha,
The maximum output range of the DAC is dependent on the VCC/VDD voltage. So, if you apply 3.3V to VDD, the maximum output range will be 0V - 3.3V. To get 5V output, you will need to apply at least 5V to the VDD input.
Thanks,
Erin