What is the maximum input analog voltage that can be measured using ADS1278. Please find the attached schematic.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the maximum input analog voltage that can be measured using ADS1278. Please find the attached schematic.
Hi Jayanthan V,
If you are using a 2.5V reference, then the maximum full-scale input voltage you can measure is VREF = 2.5V. If you apply a differential signal >2.5V, then the output code will just be the ADC max positive code (7FFFFFh)
Also, the ADS1278 has a binary twos complement coding scheme, so half of the codes are for the positive range (000000h to 7FFFFFh) and half of the codes are for the negative range (800000h to 000000h). If you are getting 7FFFFFh when you apply a signal >2.5V, the ADC is operating as intended
All of this information is in the datasheet. Please review this document in detail so you understand how the ADC actually works
-Bryan
Hello Bryan,
Kindly, help me out in understanding what is the maximum analog input voltage that can be measured with the above attached schematic.
Hi Jayanthan V,
As mentioned, this information is included in the ADC datasheet. I even provided a picture of the relevant section
Nothing that I can see in your schematic changes these requirements.
-Bryan
Hi Jayanthan V,
Currently our ADS1278 experts are out of the office until next week so be patient for a complete response. The ADS1278 is very low input impedance so you should have a driver amplifier in front of your inputs. It appears that you are directly connecting the input to a source. A more complete schematic would be helpful. Also oscilloscope shots of the input voltage would help us determine why you seeing full-scale. Most likely the input voltage is exceeding the + full-scale range. If your AC input is a sine wave (for example) centered at 1.25V, then exceeding 1.25V would reach full-scale (1.25 + 1.25 = 2.5).
See figure 90 in the datasheet for a basic single-ended interface.
Best regards,
Bob B
Hello Bob Benjamin,
I have signal conditioning circuit before connecting to ADC.
For instance, I have provided input from Regulated power supply. Input Voltage is in control, so there is no chance of exceeding the limit.
Hi Jayanthan V,
As I said in my previous post, the ones most familiar with the operation of this part are currently out of the office. You will have to wait until next week to get any additional help.
Best regards,
Bob B
Hello Jayanthan,
When using a single-ended configuration as you have shown (AINN=GND), and VREF=2.5V, the maximum full scale input voltage on AINP will be 2.5V. With 2.5V, the output code will be 0x7FFFFF.
I suggest measuring the voltage on pin 3, AINP1, to verify the actual input voltage to the ADC. With 1.25V input on pin 3, AINP1, the output code should be very close to 0x400000.

If you verify 1.25V on the input pin 3 of the ADC, and your output code is still saturated to 0x7FFFFF, then you may have a problem with your firmware. In this case, use a logic analyzer or oscilloscope and capture the /DRDY, SCLK, and DOUT signals over a full frame to confirm the correct data directly from the ADC output.
Also, for robust operation of ADS1278, remove the ferrite between the analog and digital grounds and provide a low impedance short. Ideally, the AGND and DGND are connected to the same ground plane.

Regards,
Keith Nicholas
Precision ADC Applications
Hello Jayanthan,
No, the ADS1278 does not support a 5V reference. The maximum reference supported is 3.1V.

If you need to measure voltages up to 5V, then you need to adjust your input amplifiers to attenuate a 5V input down to 2.5V.
Regards,
Keith