Tool/software:
Hello,
The datasheet indicates that the CLK pins can be driven single-ended. The datasheet is not clear on the voltage level, it only indicates TTL/CMOS. Can I drive with LVCMOS25? LVCMOS18? LVCMOS33?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
The datasheet indicates that the CLK pins can be driven single-ended. The datasheet is not clear on the voltage level, it only indicates TTL/CMOS. Can I drive with LVCMOS25? LVCMOS18? LVCMOS33?
Thanks
Hi Randall,
So the single-ended should have the same swing at the DUT power rail. So if the power rail is 3.3V, the swing should be 0V→3.3V.
Regards,
Geoff