Part Number: ADS5296A
Tool/software:
Hello,
I am integrating the ADS5296A into my design with a 160 MHz input clock and am trying to generate a 12-bit Ramp Test Pattern. Unfortunately, I am not seeing any output from the ADC, and the interleaved mode is enabled in my setup.
I have a few concerns and would greatly appreciate your guidance on the following:
1. What should the frame clock rate be? Should it match the input clock or be half of it? When I probe the clock, it is unstable, varying from 65 MHz to 80 MHz.
2. Could you please confirm the specific registers I need to configure to initiate the Ramp test pattern? Is there a specific sequence of writes I need to follow? Below are the register writes I have attempted:
- 00h: 0001h
- 00h: 0000h
- 07h: 0001h
- 40h: 8000h
- 45h: 0000h
- 46h: 8208h
- 25h: 0140h
Thank you for your assistance.
Best regards,
Akshit