Other Parts Discussed in Thread: ADS8686S
Tool/software:
Hi,
I am using an ADS8665 with the RANGE_SEL register value changed from the initial value. After setting this register, I need to wait a certain amount of time before I can get the AD conversion data I expect. Specifically, if I get data 82us after setting RANGE_SEL, the correct value is output, but if I get data 32us later, an unexpected value is output. I checked the ADS8665 datasheet, but I can't find any information about the waiting time after setting the RANGE_SEL register. Is a waiting time necessary after setting RANGE_SEL? If so, please tell me the waiting time until RENGE_SEL switches.
■ADS8665 usage conditions:
- AIN_P-AIN_GND voltage: approx. 10mV (AIN_P driven directly from op amp)
- CPHA=0, CPOL=0, SCLK: 3.28MHz
- ADS8665 register settings: Only RANGE_SEL changed, others default
■Waveform information
Thanks,
Conor