Part Number: ADS1015
Tool/software:
I am having an issue with my ADC. I am able to see the device but it is returning a value of 25. I have the gain set to 1 (4.096v) and the input voltage on channel 0 is 3.26v (verified with a multimeter) but the output is ADC value of 25 or 0.025v. All 4 channels output incorrect values.
I noticed there is a lot of undershoot but I am not sure if that is just error from my oscope leads or probe placement. I noticed there is a ? at the end of the decoding as well.


Any help would be appreciated.
Thank you!