ADS1291: LOFF_STAT Register Always Returns 0 When Read Individually

Part Number: ADS1291

Tool/software:

Hello, 

I'm currently running into a problem when trying to read the LOFF_STAT register after switching from AC leads configuration to DC leads configuration, where it always returns 0. However, when streaming with DC leads configuration enabled, the LOFF_STAT register in the STATUS portion of the stream returns the correct value. Additionally, when changing the configuration back to the AC leads configuration and reading back the entire configuration, it returns the correct value as well. 

The AC Leads configuration set by default sets the registers to the following values: 

// Binary Register Selected Options
// -----------------------------------------------------------------------------------------------------
CONFIG1: 0x03,     // 0b00000101 Continuous, 1000SPS
CONFIG2: 0xF0,     // 0b11110000 Test signal disabled, Internal *4.033V ref enabled, Leads Off enabled.
LOFF: 0xF5,            // 0b11110101 70%-30%, 22 nA, AC lead off frequency F_DR/4
CH1SET: 0x00,        // 0b00000000 6x Gain, Electrode input
CH2SET: 0x81,        // 0b10000001 Power down, Input shorted
RLD_SENS: 0xE0,   // 0b11100000 fMOD / 4 Chop Frequency, Buffer Enabled 
LOFF_SENS: 0x03,  // 0b00000011 Enable positive and negative
LOFF_STAT: 0x00,   // 0b00000000 Read-only
RESP1: 0x02,           // 0b00000010 N/A
RESP2: 0x07,           // 0b00000111 N/A
GPIO: 0x00,              // 0b00000000 Output low

Then we change the configuration and read registers using the following process: 

1. Set PWDN/RESET low
2. Wait 8uS
3. Set PWDN/RESET high
4. Wait 36uS
5. Send SDATAC command 
6. Wait 8uS
7. Wait an additionally 0.9S, then set LOFF to 0xF4
8. Wait 502mS, then read LOFF_STAT
9. Wait 1ms then set LOFF_SENSE to 0x13
10. Wait 502ms then read LOFF_STAT
11. Wait 1ms then set LOFF_SENS to 0x03
12. Wait 502ms then read LOFF_STAT

Is there any reason why reading the LOFF_STAT register individually with the configuration above shouldn't work? 

All delays other than the 8uS and 36uS are necessitated by unrelated code, but I included them in case they could be helping/hurting the problem. 
All LOFF_STAT reads described above return 0 despite the LOFF_STAT portion of the ECG stream returning 1 in the proper bits when streaming is enabled with the same hardware configuration. 
I haven't included included my process for setting the register initially, but I include all of the delays described on page 40 of the ADS1291 datasheet (to my knowledge), and when reconfiguring back to the standard configuration above after this process, the LOFF_STAT register returns 1 in the proper bits. Lastly, if instead of only writing to individual registers, if I rewrite the entire configuration block instead of writing to individual registers each time under DC lead detect mode, I still read only 0s in the LOFF_STAT register, but I believe I have other problems there as well, as it then acts like stop continuous mode didn't work after re-writing the configuration, but I haven't dug into that too deeply. 

My question is, is there anything I'm missing? Is there any reason why it would work in the streamed packet and not while reading an individual register/with the configuration I have? Is there any reason why rewriting the entire configuration at the end with all delays and resets shows the LOFF_STAT register values as 1 when the previous reads with the previous delays didn't return the right value? 


  • Hello Lindsey,

    Thank you for your post.

    Just to confirm, the LOFF_STAT bits in the STATUS word are correct when you are streaming the data (i.e. RDATAC mode), but not when reading the LOFF_STAT register directly? What happens if CLK_DIV is set to 1b (bit 6) - does the entire register still read back as 00h?

    The LOFF_STAT bits should only be read when using DC lead-off detection. The comparator outputs are not valid during AC lead-off.

    Regards,
    Ryan

  • Hello Ryan, 

    Yes, the LOFF_STAT bits in the STATUS word are correct in the streamed data packet, but not reading the LOFF_STAT register directly. When setting the CLK_DIV bit to 1 (i.e. writing 0x40 to LOFF_STAT), the LOFF_STAT register returns 0x40 in all above configurations. I'm only reading this register when the device should be in DC lead-off detection mode, which I believe should be configured by setting LOFF to 0xF4. 

    I've attached some scope captures of reading the LOFF_STAT register in the streamed packet as well. The first one LOFF_STAT returns 0 in all IN1N/P fields with the configuration described in step 10, and the second one properly shows the IN1N field as 1. I realize now that I missed 2 minor steps in my configuration, and I'll add the updated steps below. 

    1. Set PWDN/RESET low
    2. Wait 8uS
    3. Set PWDN/RESET high
    4. Wait 36uS
    5. Send SDATAC command 
    6. Wait 8uS
    7. Wait an additionally 0.9S, then set LOFF to 0xF4
    8. Wait 502mS, then read LOFF_STAT
    9. Wait 1ms then set LOFF_SENSE to 0x13
    10. Wait 502ms then read LOFF_STAT
    11. Change hardware configuration to allow DC leads signal to pass through
    12. Wait 502ms then read LOFF_STAT

    13. Wait 1ms then set LOFF_SENS to 0x03
    14. Wait 502ms then read LOFF_STAT



  • Hello, is there any update on this issue?

  • Hi Lindsey,

    I do not see any issues with the register configurations. 

    In Step 11, you are changing the hardware to allow for DC signals - are the inputs AC coupled prior to this step? In Step 7, you are configuring the device for DC lead-off correctly and reading from the LOFF_STAT register. The inputs have to be DC coupled for this to work. Am I misunderstanding what is happening in Step 11?

    Another thought - it seems the LOFF_STAT bits in the STATUS word are correct when streaming data. I assume the register settings remain constant during data capture and the input voltages have time to settle after disconnecting an electrode. In contrast, when you configure the LOFF and LOFF_SENS registers, and then read LOFF_STAT ~0.5s later, perhaps the input voltage has not yet been pulled above or below the comparator thresholds. Can you try waiting longer to see if that's the case?

    Regards,

    Ryan