Tool/software:
Dear Specialists,
My customer is evaluating ADC08D1000 and encountering the problem.
I would be grateful if you could advise.
---
I'm encountering an issue with the ADC08D1000 where the settings differ from the circuit wiring when the power is turned on.
I'd like to confirm the specifications of the ADC08D1000's 14-pin (FSR/ECE) terminal.
According to page 11 of the data sheet
Low: Full-scale differential input 650mVp-p
High: Full-scale differential input 870mVp-p
When the power is turned on, it should operate at a full-scale setting of 870mVp-p, but sometimes it becomes 650mVp-p.
Currently, the wiring for pin 14 is shared with the power supply circuit.
I think this connection may be causing the problem.
Could you please tell me the voltage conditions for recognizing High and Low in normal control mode and the timing for reading the settings?
ーーー
I appreciate your great help in advance.
Best regards,
Shinichi