Part Number: ADS131E08
Tool/software:
Hey Precision ADC Team,
I have a customer evaluating the ADS131E08 for a project and we were hoping you could help to provide guidance on a couple questions related the reference input voltage and overall measurement range. Please see the testing conditions and questions below!
AVDD = DVDD = 3.3V
VREFP = 2.4V, configured as an output
VREFN = AVSS = 0V
VINxP = ranges from 0V to 2.4V
VINxN = 1.2V
PGA gain = 1
Based on the differential input voltage specs in the Recommended Operating Conditions of the datasheet, are we using the full measurement range of the ADC? If we were able to supply 5V to AVDD, would we be able to increase VINxN to 2.4V and VINxP up to a range of 0V - 4.8V? If so, is there any benefit to doing this, instead of just increasing gain to 2?

Best regards,
Matt Calvo