Part Number: TX7332
Tool/software:
Hi,
I have a few technical questions about TX7332 output capabilities:
- Can TX7332 support different pattern profiles per channel? That is, can it transmit unique patterns on different channels at the same time?
- How long can TX7332 support 5W per channel output time-averaged power? I’m wondering this since it appears that the IC can support peak power of up to 100V*1.2A, but am not sure at what point thermal shutdown would occur for different power levels.
- What output fundamental frequencies can TX7332 support? Can TX7332 support 600kHz and 200kHz center frequencies if I wanted to output square waves, for example?
Thanks!