Other Parts Discussed in Thread: LMK04828
Tool/software:
Hi,
I am trying to use the TI_JESD204 IP in vivado to programme my ZCU102 to work with this DAC but it just had no output. The board is tested without problems. I think it's just because I have some trouble with the clocking setting. I
I tried to follow the clocking set of this one TI_JESD204_IP_KCU105_DAC38J84_841.zip but the I am confused why the external clock frequency is 409.6MHz. And why is the DCLK divider in the tutorial is set to 32?
I used 156.25MHz external clock and the clock output from CLKout 12 is just 156.25/(Divider I set) MHz which I used as the sys_clock.
Here's the DAC's setting.