Part Number: ADS8588S
Tool/software:
Hi Expert,
The output codes from ADS8588S are as below form:
| input voltage |
output code |
|
0.01V |
0x 00F6 |
|
2.49V |
0x 7FBE |
|
2.51V |
0x 80C2 |
|
4.99V |
0x FFB0 |
When the input voltage is over than 2.5V, the output code is overflow. You can see the code of 2.51V is start with "8".

Below is the schematic, could you please help analysis the issue?
They use internal REF, set PGA RANGE to +-5V.

BR,
Moon
0.01v input
2.49V input
2.51V input
4.99V input