Other Parts Discussed in Thread: ADS1213, DAC8871
Hi people:
When i made my prototype board i used the data converter ADS1213P (24 pins DIP Version) and the Vbias was zero, before enabling it via internal register. However, now, in the final version, im using the ADS1213E (28 pins SOIC Version) and now the Vbias is 3.3V at power up (without enabling the register), is this normal? is this a feature of this version?
I want to be sure about that, because i dont want to run into strange issues when the final prototype is running. (And i havent found information about this specific case)
Are there any other major differences between the parts?´
Thank you very much and best regards