Hi,
I am planning to use the DAC7741 EVM to dirve the input of a piezo amplifier. The specifications of the DAC7741EVM state that the supply voltage for the analog section must be +-15V. Is it ok if I supply +-12V instead? I believe that doing so will only limit the rail to rail voltage of the opamp in the EVM and eventually will reduce the output range of the EVM. Is this correct or will providing +-12 V stop the EVM from working completely?
Thanks.