This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dean,
I have some questions about the input clock of the DAC5670(DACCLK_P/N).
1.Can the chip DAC5670 accept the LVDS clock (DACCLK_P/N) directly ? What the datasheet said "Page 9. DACCLK_P/N Clock differential input voltage :200-1000mv;DACCLK_P/N Clock common mode:1.0-1.4v" is consistent with the LVDS standard . But the page 21 said"The DAC5670 features differential,LVPECL compatible clock inputs (DACCLK_P, DACCLK_N)".
2.if i use the LMX2581 to generate clock for the DAC5670(DACCLK_P/N),what is the net i need to add between the output of the LMX2581 and the input of the DAC5670(DACCLK_P/N) ?For the output of the LMX2581 is sine wave ,but the "DACCLK_P/N" is digtal input.
Regards,
Lei