Hi,
Please send me password for source code ftp://ftp.ti.com/pub/data_acquisition/ECG_FE/ADS1298/Source_ads129x_v1p1.zip
My email id is rahul.amu2@gmail.com
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please send me password for source code ftp://ftp.ti.com/pub/data_acquisition/ECG_FE/ADS1298/Source_ads129x_v1p1.zip
My email id is rahul.amu2@gmail.com
Thanks
Hi Rahul,
We'll contact you shortly.
Hi Tom,
Please send me the password at high priority. It is very urgent for me. If you don't have the source code for the software of ADS1298ECGFE , then please clearly tell me
Thanks
Hi Tom,
Can you send me the password Please? my email juliansalda85@gmail.com
Thanks.
Hello Tom, May I know the passcode as well? I need access to those files as well
conexy@163.com
Many thanks
Hi Tom,
Please send me the password at high priority. It is very urgent for me. If you don't have the source code for the software of ADS1298ECGFE , then please clearly tell me
jaballimaher@yahoo.fr
Thanks
Mr Tarek -
You should receive an email shortly with the requested information.
I would like to receive the password to ftp the Source_ads129x_v1p1p1A.zip file.
Also, I'm in trouble to dowload the "ftp://ftp.ti.com/pub/data_acquisition/ECG_FE/ADS1298/ads129xecg-fe-setup-1.1.1.exe" file.
Can someone help me ???
Thanks in advance.
Carlos Jaccoud
Email: jaccoud@superig.com.br
Mr Jaccoud -
We can get you the password for the source files. May we use the email address in your profile to contact you?
Regarding the software, there apparently are some problems getting the software from the ftp site currently. We are working to try and resolve this problem and hope to have something in the near future. We are looking into a short term solution, but this needs to be investigated further.
Mr Jaccoud -
Can you please check the link for the software again to see if it works for you now?
Hi Tom,
I also need the password,please email to me.thanks!
email addr: duanfurong@jovian.com.cn
I have try to download ads129xecg-fe-setup-1.1.1.exe many times.but all failed to download.please email this software to me also.Thanks
best regards.
rose duan
Rose -
You should receive an email shortly with the requested password.
Unfortunately, we cannot email the software due to the size of the file. Please check your internet access/firewall settings to make sure you can access the information.
I need to download the software ftp://ftp.ti.com/pub/data_acquisition/ECG_FE/ADS1298/ads129xecg-fe-setup-1.1.1.exe from the ftp server. Could you please assist me with the username and passkey. Thanks in advance.
philipvaliyil@gmail.com
Regards,
Philip Joseph
I am unable to download the software installer for the ADS1298ECG-PDK evaluation board. Would you be able to provide instructions or username/password information to access these files from the ftp site (ftp://ftp.ti.com/pub/data_acquisition/ECG_FE/ADS1298/ads129xecg-fe-setup-1.1.1.exe/). If possible I would also like to download the source code. My email is ricardo_a7@yahoo.com. Thank you for you help.
Please check your firewall settings to make sure that you can access the site. We have run across conditions where the your firewall/company is prohibiting access. We have check locally and the file can be accessed properly.
Additionally, if this doesn't work, can you provide a screen capture of what you get when you try and access the file?
Hello Greg,
Thank you for the quick response. I have tried turning off the firewall and used two separate computers on different networks with different browsers. When I click on the software download link (under http://www.ti.com/tool/ads1298ecgfe-pdk) the browser seems to keep trying to connect without any results for longer than 30min. The firefox status shows: Transferring data from teasinstrument.122.2o7.net.. I have also tried to access the ftp files using filezilla, the windows documents managers, saving the link directly to my computer, etc. but I do not get through. I am assuming that there is no password to access the installation file. (Or should we be using a specific username/password to access the files) Thank you.
There should not be a password on the installer, so this is not the issue. Is your connection speed fairly high? The installer file is ~ 165MB so it is possible it could take a while to download, depending on your connection speed.
Hello Greg,
My internet download speed is >25Mbps which would definitely download the file in under 30 minutes. When I save the link as a target file to my computer it always shows 0 Bytes. It does not start the download. Is there any other way to download the file? (Maybe a mirror site or by ordering a CD). Thank you
Dear Greg Hupp:
Please send me password for Source_ads129x_v1p1p1A.zip. It is very useful for me.
My Email: zhanglei@ahu.edu.cn
Thank you very much
Hi,
Please send me password for source code ftp://ftp.ti.com/pub/data_acquisition/ECG_FE/ADS1298/Source_ads129x_v1p1.zip
My email id is songxing.frank@gmail.com
Thanks
Hi Frank -
You will receive an email shortly with the requested information to the above address
Hello,
Can I ask for passcode for ftp://ftp.ti.com/pub/data_acquisition/ECG_FE/ADS1298/Source_ads129x_v1p1.zip?
My email is niki_dobro@abv.bg
Thanks and Regards
Nicky