This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Current consumption on SM28VLT32-HT

Other Parts Discussed in Thread: SM28VLT32-HT

Hi,

The current is specified for the Core and I/O rails on page 4 of the datasheet for the SM28VLT32-HT part, , however it is a little unclear to me. Can you confirm that these numbers are correct:

  • Erase current - Core + I/O: 1.8V * 127 mA + 3.3V * 76 mA = 480 mW
  • Program current - Core + I/O: 1.8V * 127 mA + 3.3V * 85 mA = 510 mW
This seems like a lot of power and might be prohibitive for some of our customers designs.
Thanks!
DJ