This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'd like to confirm Timing Requirements for Serial Write Operation.
Test conditions show as followings on the data sheet(on Page7);
<Timing Requirements(correct values)>
In case of AVdd = 3.3V,
1. SCLK cycle = min 50ns
2. SCLK high time = min 25ns
3. SCLK low time = min 25ns
<Question>
If input SCLK pulses(cycle, high time and low time) are shorter as like -Example conditions- than above values ,
does the DAC8411 output false values, or not at all?
If you know, could you tell us?
-Example conditions-
SCLK cycle = 45ns
SCLK high time, low time = 22ns
Then, we promise that we never use under <Example conditions>.
We know this is illegal direction.
Hirorotaka Matsumoto
Hello Matsumoto-san,
The DAC8411 SCLK is guaranteed to work at a minimum of 50ns SCLK cycle time with AVDD = 3.3V. There is small headroom, but due to process variations any smaller cycle time cannot be guaranteed to work as expected. We cannot predict if the part will work correctly, latch in the wrong value or simply disregard the command.
Regards,
Hello Eugenio San,
Thank you for your reply and your kindness.
We understood your saying completely.
Kind regards,
Hirtotaka Matsumoto