All:
I have done minimial work with the board, but I was able to demonstrate a very clean ECG waveform on the TI GUI by attaching the board to a laptop running on battery power and a patient simulator also running on battery power. Very impressive - by the way, I have the ADS1292R chip on my board.
I am impressed with the capabilities you have been able to squeeze into the board, especially with the MSP430!
Some ideas:
The board, even though small, could be made even smaller, especially if you use the F5528 package instead of the F5529 package. Also, I would like to see the smallest footprint of the ADS1292R put on the board. I am working in an environment that thrives for the smallest form factor that can be done. By having these two pieces of the board in the largest modules, it may actually make the sales portion a bit tougher...