I have a customer who would like to use the VBAT1 and VBAT2 on the TSC2003 to measure up to 32Vdc. Since there are built-in resistor voltage dividers on each input, could he simply just put a 47.5k ohm resistor between the sensing pin and the voltage he wants to sense and be safe? The datasheet states that the max voltage on either VBAT pin should be less than 6V, but with the voltage dividing resistors activated, the voltage at those pins should be approximately 5.56V. Thanks for your help.