Hello,
I have two DAC37J84 Eval cards connected to two FMC connectors on a Xilinx VC707 FPGA Eval card. Using the TI DAC setup GUI, I setup both eval cards with external clock and drove both with a 983.04 MHz clock, no problem.
My JESD Verilog program has a JESD204 phy layer driver for each DAC37J84 Eval card, those also work well.
The problem is synchronizing SysRef to each of the two DACs. I generated a 800 nsec. pulse, and sent it to pin 6 SYNC input of each LMK04848 (I may have that part number wrong but you know what I mean) clock cleaner chip (one on each eval card), However I can't figure out what to set the LMK SysRef Mux and Sync modes to. Would you please recomend the LMK setups I need? I really appreciate your help
Thanks,
John Reyland