Other Parts Discussed in Thread: AFE4490, CC2541, ADS1293, CC2640
Hi,
I am trying to interface AFE4490 for pulse oximetry by designing a custom board. The AFE4490 is not being able to generate any signal on TXN and TXP pins.
I have set all supply voltages as 3.3 V.
The voltages on various pins are as follows:
BG = 0.98 V
TX-REF = 0.68 V
VCM = 0.97 V
TXN = 2.52 V
TXP = 3.3 V
I am being able to see the signals on MOSI and MISO pins when I try to write and read registers. Also, the CLK_OUT of 4 MHz is being observed from the AFE4490. But, there is no signal on the ADC_READY pin.
Please help!
Thanks in advance.