Other Parts Discussed in Thread: TIPD188, DAC7760, MUX36D04, TS12A12511
I am working on a new PLC weigh indicator design using the ADS1262. The TIPD188 Reference Design was very helpful. However, most of the load cell strain gauges in the industrial space are still using 1mV/V sensitivity, which at 5V AC Excitation would half the overall measurement resolution. Most Load Cells recommend using at least 10V-15V Excitation voltage to compensate for this. Since the ADS1262 is controlling the 5V AC excitation, do you have any recommendations on how you recommend designing 10V AC Excitation using this ADC?