Other Parts Discussed in Thread: , ADCPRO
Problem: Chop function.
(1) In the ADS1263 datasheet, there is no explanation of the chop techniques used. The only note is in Sec. 9.3.6 (The PGA consists of two chopper-stabilized amplifiers...).
(2) In Sec. 7.5, general conditions, there is no definition of chop mode used. The only note appears at Offset voltage and Offset voltage drift. Does this mean that all the specifications in Sec.7.5 belong to both modes, chop mode ON and chop mode OFF ?
(3) Specifically, the noise tables in Sec. 8.8 belong to both chop modes ?
(4) When experimenting with the ADS1263EVM-PDK, Tab 3: Digital filter shows two windows ADC1 Data Rate. When chop is disabled, the figures in both windows are the same, e.g. 400 SPS and 400,0Hz, regardless of the ADC1 filter type. When chop is enabled, the figures are different, e.g. 400 SPS vs. 391,8Hz with filter Sinc1, 197,9Hz with filter Sinc2, 132,4Hz with filter Sinc3, and 99,5Hz with filter Sinc4. Now, what is true? There is no explanation of this behavior in the ADS126xEVM-PDK Users´Guide.
(5) When experimenting with the ADS1263EVM-PDK, is there any possibility to prolong the programmed acquire alert of 30,0 sec ?
Thank you for your response.
Best regards,
Jiri Dostal