This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7826: VREF(Max) at Vcc = 3.3V

Part Number: ADS7826

Hello,

My customer has a question about ADS7826.

[Q]

In the data sheet of the ADS7826, it is stated that VREF(Max) = Vcc - 0.2 V at  Vcc = 2.7 to 3.6 V.
My customers want to use Vcc 3.3V.
Is it possible to use the circuit of Figure 40 in the data sheet at this time?


Best Regards,

Kaede Kudo