Part Number: TSW14J56EVM
Hello,
I'm using ADC12J4000_D4_DDR profile and noticed it has two channels and data that is captured is almost identical in both of them and so it effectively makes it 1G of samples I would like to use whole 2G samples with decimation I tried to change number of channels in INI but it seems like not giving me appropriate output I suspect there is something that I need to change or don't understand?
Unrelated to this I found an issue with HSDC GUI if I capture 2G of samples 4GB temp file is created ADCTempX.bin (X - channel number) in HSDC folder but when I save samples from UI only first 2GB is copied into destination file looks like UI logic sees 1 channel and assumes max channel size is 1G (2GB). I ended up using temp file as of right now but just wanted to let you know.
Also can I change somehow analysis window size beyond 512K samples?
PS: I'm using HSDC GUI version 4.50.
Thank you,
V.