Dear Sir
I am referring TI design to design
1. Does ADS8688 have layout guide ? Beside datasheet
2. If we have below circuit ,does this circuit have component RC size suggestion ??
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
1. You can also look at the EVM User Guide for the ADS8688 for an example of PCB layout. Keep in mind that the TIDesign is designed to comply with IEC61000-4 Standards, if this is an aspect you are concerned with, I would suggest closely following the TIDesign layout.
2. As for the RC, the RC used in the design is verified to work properly. The attached power point is a presentation that you may use to learn more about how to drive a SAR ADC input. It covers using an op amp and RC value selection.
Summit - 2017 Part 2 - Driving the ADC - 5-17-2017_TG.pptx
Regards
Cynthia