Part Number: TSW1400EVM
Other Parts Discussed in Thread: CDCE62005
I need to use the SYNC1 or SYNC2 output from the TSW1400EVM to drive the ~SYNC input to the CDCE62005 on the DAC3484EVM.
I have configured the TSW1400EVM to pass my external trigger signal to the SYNC1/2 connectors appropriately, but there does not seem to be any way to invert this signal. Since the external trigger in the TSW1400EVM FPGA reacts to the rising edge, I cannot invert my external trigger signal. I need the CDCE62005 to be synchronized to the same edge.
Is there a command to invert the SYNC1/2 signal outputs in the TSW1400EVM FPGA? If not, can such a thing be added?
Thank you!