This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi.
I am designed ADC32RF45EVM board and KCU105EVM Board.
ADC32RF45EVM With KCU105 Board Setup Example in "HSDC Pro With Xilinx® KCU105 User guide (SLAU711–March 2017)"
Set up the hardware as follows:
1~9 is ok.
but, "10. Open HSDC Pro, select the ADC tab, and select "ADC32RF34_8224" using the drop-down menu" is not supported in HSDC Pro 4.70.
but, i can't see "ADC32RF45_8224" in drop-down menu.
i want to this example completed.
what is problem?
Help me please.
im,
It looks like 2 INI files for ADC32RF45 did not make it into the HSDC Pro release. I have attached the missing INI - can you please put this into the ADC Files folder and see if it works ok?
C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro\KCU105 Details\ADC files
Ken.
hi ken C
thank you for your help.
i will try .ini file and reply result as soon.
thank you very much.
Kim,
Did you load the FPGA using Vivado before running HSDC Pro? What is the status of the LED's on the KCU105? What configuration file did you load the ADC EVM with? Can you send a screen shot of HSDC Pro GUI?
Regards,
Jim
hi Jim,
thank you for your reply.
1. i'm download “C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro\KCU105 Details\Firmware\KCU105_TI_DHCP.bit".
2. KCU105 Board Status and User LEDs are all green. (DS2-init, DS3-OR'D POWER GOOD, done....)
3. adc32rf45evm configuration file? i'm bypass mode setting in GUI.
"HSDC Pro With Xilinx® KCU105" file version SLAU711–March 2017. see it
Regards,
Kim
Kim,
1. We need to make sure if the FMC Voltage is set as per page 8 in KCU105 User's Guide
2. DCLK Divider in the ADC should be set as required as per point 6 and 7 in page 19 in KCU105 User's Guide
Regards,
Jim
Kim,
Is your setup now working? I cannot tell by your latest response.
Regards,
Jim
hi ken,
I am designed ADC32RF45EVM board and TSW14J56-REV D EVM Board.
and High Speed Data Converter Pro v4.70 -> v4.00 down-grade.
i'm example project completed. but, ADC32RF45EVM board and KCU105 Board are still does not work.
"ADC32RF45_8224.zip" file is a very usefulled for me.
thank you very much.
Regards,
kim